Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX Monthly Update (NX 1859) is available for download

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

@BenBroad 

I am not able to send you a PM, therefore replying here.

Difficult to tell why there's no other reports against the issue. Could be that Russian customers are not moving to NX CR en masse yet. The issue was discovered at our office when we started to test NX CR in response to the actual customer's request. It was duplicated on all machines at our office. I then opened an IR and it was duplicated at the Russian Siemens office. So at our side at least the existence of a bug has been confirmed independently multiple times.

Re: NX Monthly Update (NX 1859) is available for download

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00 !

 

A few things I have seen cause Uncompress to run slow:

 

- Running Uncompress with ZIP file residing on an external drive

- Similar if using a network mounted/mapped drive

- Running in a folder that is  being monitors by realtime Virus Checker

 

 

 

Re: NX Monthly Update (NX 1859) is available for download

Phenom
Phenom

Hi @BenBroad ,

before to all, sorry for the big mistake. English is not my language.

When I wrote :

'...Unzip 7 gb (NX1859) is done in 2 minutes, but the update (missing word) .msp (1 gb) need 23 minutes....'

I thought that the .msp use the same strategy to update NX as before.

My report is that I would like the future automatic update as fast as possible.

Thank you...

Using NX1867
RuleDesigner PDM

Re: NX Monthly Update (NX 1859) is available for download

Phenom
Phenom

Hi @PatMcManus ,

I didn't was clear. Sorry. I respond here.

Thank you...

Using NX1867
RuleDesigner PDM

Re: NX Monthly Update (NX 1859) is available for download

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00 !

 

No need to apologize. I am a native speaker and still sometimes make those sort of mistakes but have no excuse!

 

I was finally able to get to my upgrade this morning with the April update.

 

My total time was roughly 6 and 1/2 minutes (6:35 =>1:20 to "check", 0:25 to "calculate space", 4:15 to "copy new files", and0:20 to "remove backup files").

 

I assume time would vary somewhat depending on the HW, disk speed, HDD vs. SDD, other apps installed, state of the registry, etc...

 

By comparison, I did some timing tests for the Install Team when we released the first update in Feb and on this same machine the total time was close to 4 minutes. I am told that will depend on how many files we update, so maybe a few more this time around.

 

I skipped March update because I was traveling, so no numbers for that.