Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Topology Optimization for NX 1847 series is available from GTAC

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

Pleased to announce that the NX 1847 compatible version ot NX Topology Optimization for Designers is available from the GTCA Download page.

      NX, NX 1847 Series, Add-Ons, Topology Optimization for Designers


t1.jpg

 

… and yes this does work in NX 1851

 

Installation document included in the zip file.

 

 

Guy Wills

Topology Optimization Product Manager

 

Guy Wills
7 REPLIES 7

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Honored Contributor
Honored Contributor

Can the application and startup folders be placed in the ugii_site_dir, so that it is available for all users?

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @DaveK 

 

The last line in the installation.docx file states:

"UGII_USER_DIR has been quoted here, but equally the UGII_SITE_DIR env var location maybe used."

 

Regards, Ben

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Honored Contributor
Honored Contributor

Thanks Ben, I should have scrolled just a bit more.

-Dave
NX 11 testing NX1847+ | Teamcenter 11 | Windows 10

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Experimenter
Experimenter

Guy,

This is Pete Patel from JPL NASA.

I am getting an error message "No material assigned to a design space or a scenery body". I have checked, material is assigned. I believe it is checking for "Setup Info" and I must have missed something in a model or not following proper sequence. I have following in in my simple model.

1. One solid body with Simple hole (Fixed) and Counterbore hole (load). 

2. In design space, I have defined Design constraints, Optimization Features and Load case.

3. Material is assigned from NX library.

4. When I click on Setup Optimization, I get an error.

What I am missing? 

Successfully, I have ran couple models but I can not figure out in this case. Any help?

 

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @Pete_jpl 

 

Can you open an IR with GTAC and send them the part to investigate this issue.  We have some PR's that were opened with the same message that were fixed in NX 12.0.2 and require the latest patch from the FTP server:

 

Screenshot - 4_23_2019 , 8_54_24 AM.png

 

These PR's seem to be related to a specific option in the material attributes section of the customer defaults, so I question whether your issue is the same as you mention that you've already successfully completed the task on a couple of parts.  Let me know if your customer defaults are any different to the following:

 

Screenshot - 4_23_2019 , 9_01_02 AM.png

 

Regards, Ben

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Legend
Legend

Hi @Pete_jpl ,

We had the problem you talk about.

We raised an IR months ago and the solution that is described by @BenBroad worked for us !

Best regards,

Frédéric.

Re: NX Topology Optimization for NX 1847 series is available from GTAC

Experimenter
Experimenter

Ben,

Setting environments for Material worked. Thanks a million.