Cancel
Showing results for 
Search instead for 
Did you mean: 

NX VB Journal

Pioneer
Pioneer

Has anybody every run a checkmate class (%mqc_update_all_features to be exact) from a VB journal and captured the result in a txt file?

 

Thanks for any help or advice in advance,

 

R

3 REPLIES 3

Re: NX VB Journal

Siemens Genius Siemens Genius
Siemens Genius

Why the journal?

Is it because you are wanting to run in batch (Check-Mate already can) or the results txt file has to be in a specific format, different to what the Check-Mate log offers?

Re: NX VB Journal

Pioneer
Pioneer

Hi,

 

Yes, i need to validate a large about of data (3rd party data) checking that the features update is just one element of it.

 

R.

Re: NX VB Journal

Siemens Genius Siemens Genius
Siemens Genius

I guess there are a couple of things that may be useful.

 

First there is running Check-Mate from a command line:

Check-Mate from a command line

 

Second there is running Check-Mate on TC import:

Examples for using validation options

 

Does that help?