Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Viewer Licensing Error

Valued Contributor
Valued Contributor

Hi,

trying to run NX Viewer (NX11.0.1.mp1) I get this error. There is no menu to select Bundles.

 

2017-04-20_11h55_36.png

6 REPLIES 6

Re: NX Viewer Licensing Error

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @dziubelis,

 

You can set the bundles before you start NX (viewer).

Either use the variable:  UGS_LICENSE_BUNDLE=

 

Or the preferred way: in Windows, Start --> Siemens NX 11.0 --> NX Licensing Tools --> License Tool --> Select the appropriate viewer bundle.

Close the menu, and start NX (viewer)

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX Viewer Licensing Error

Valued Contributor
Valued Contributor
So its not bundled with NX, you have to actually buy seperate license for Viewer?

Re: NX Viewer Licensing Error

Legend
Legend

Nothing is free...

 

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX Viewer Licensing Error

Valued Contributor
Valued Contributor

Thats not true, especially if we have viewers in mind Smiley Wink

Re: NX Viewer Licensing Error

Siemens Phenom Siemens Phenom
Siemens Phenom

That is correct, NX viewer Checks out a sepparate cheaper license. But it is actually a separate license, that needs to be purchased.

 

If you want a free viewer, you could have a look at JT2Go or XpressReview.

 

Hope this helps,

 

Kind regards,

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX Viewer Licensing Error

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

NOTE: (unless Siemens fixed it):

Once you use the "License Tool" to set the bundle, the ENV is ignored, unless you delete the registry entry that the license tool uses (you can't just de-select the bundle in the license tool).

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled