Cancel
Showing results for 
Search instead for 
Did you mean: 

NX Viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Good Afternoon every body

 

If I want to install NX Viewer

Should I use NX Base Installer to install NX Viewer only (we don't need another feature) ?

or

Is there any special for NX Viewer Installer?

Thank you in advance

 

Dadang

 

3 REPLIES 3

Re: NX Viewer

Valued Contributor
Valued Contributor

NX Viewer should be in your Windows start menu under Start /All Programs/Siemens NX 10.0/NX Viewer

This pertains to NX 10 & 11, and should be the same with older versions.

Re: NX Viewer

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @dw89mk,

 

@akrenzer is right, after you have installed NX you will find the option, in your Windows Start menu as explained.

 

About the installation itself. You can just download the full NX install (there is no separate NX viewer installer). Run the installer, and select the option you want to install from the installation menu.

 

When installed, you will find the NX viewer shortcut in the windows Menu.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX Viewer

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Dear Akrenzer and Dennis,

 

Thank you for your help

 

Kind regards,

 

dadang