Cancel
Showing results for 
Search instead for 
Did you mean: 

NX and TcSim

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

I need an education.  I hear the term TcSim used often in connection with Simulation, but on the GTAC download site, I see Simcenter 3D and Simcenter Nastran.  

 

Under the NX download page and Add-ons, I don't see sim-anything.

 

Can someone explain the terminology for me?  What the different sim's are and if using the TcSim term is even correct are there yet other simulators that I haven't mentioned here?

3 REPLIES 3

Re: NX and TcSim

Siemens Phenom Siemens Phenom
Siemens Phenom

Simcenter 3D is a CAE pre and post processor

Simcenter NASTRAN is one of the solvers Simcenter 3D can use

TcSim Teamcenter for Simulation helps you manager the data created by simulation packages.

Steve V

Re: NX and TcSim

Solution Partner Experimenter Solution Partner Experimenter
Solution Partner Experimenter

Thanks that helps.  Under the Teamcenter download I don't see TcSim as an added module and  I don't see it under Integrations and Solutions, is it part of core Teamcenter?

Re: NX and TcSim

Legend
Legend

Hi @kvanderstel 

I think so, or at least some of it is included in the main Teamcenter download. Without any add-on or any feature installed you'll have access to some applications and to go further in TEM you'll be able to check-in those features :

 

2019-08-15_145838.png

 

Best regards,
Frédéric.