Cancel
Showing results for 
Search instead for 
Did you mean: 

NX attributes in properties from explorator windows

Pioneer
Pioneer

Hello again,

Does anyone know, how to write nx attribute values as Windows file properties?

I want to set the attribute bar in file property in explorator windows like on the picture below. 

atributes.jpg

 

I will be very happy, if someone know how solve this problem.

4 REPLIES 4

Re: NX attributes in properties from explorator windows

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom
did you test to try settings some NX properties and then save the part.
after that check you windows file again.

it looks that is shows in your picture some default NX properties.

Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX attributes in properties from explorator windows

Pioneer
Pioneer

Yes, I probably checked all options in nx. I think, that it will be working when I change  a .dll file. But here is a problem, because I don't know which file I must change and how can I do it? 

 

I found this:

The display you see in Explorer is apparently constructed by Explorer itself. It can

do this because it knows how to look inside certain types of files and

find the info it needs. One solution is a thing called dsofile.dll

 

But this file is suitable to Office only, if I think correctly :/

Re: NX attributes in properties from explorator windows

Phenom
Phenom

as I remember, there was a UGS .dll for this until NX5, that one had to register.

I used that for a while, it was pretty dangerous though, I remember that whenever

I tried to perform some file operation (copy, rename, etc.) within the NX Open file

dialog then NX quitted abruptly.

Re: NX attributes in properties from explorator windows

Pioneer
Pioneer
Okay, thanks for help. I'm trying to do something through NX Open, but I still do not know exactly what I need to change to set these attributes.