Cancel
Showing results for 
Search instead for 
Did you mean: 

NX crashes on inserting section view

Pioneer
Pioneer

Hi,

 

When I'm trying to insert a section view for a particular drawing file, (TC integrated) NX crashes.

Other views I'm able to insert without issues. This issue is present in all machines.

Syslog only shows below error:

!!!&MACRO EVENT FOCUS_IN 0 0, 327680, 0, 0, 0! (Application CB Nested)
!!!&MACRO ASK_ITEM 327680 (1 OPTM 0) = 0 ! Dynamic
*** ERROR: Unhandled exception: 0xc00000fd at Fri Dec 14 09:20:36 2018 Eastern Standard Time
*** ERROR: Stack overflow

 

Any clues as to how to check this issue.

3 REPLIES 3

Re: NX crashes on inserting section view

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Try to test it native.

So that you can find out if it is NX related or TC related.

Re: NX crashes on inserting section view

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You'll probably have to report this to GTAC along with the files.

 

You could try running a part cleanup (see other threads) - on all open parts or assembly or ?

Save all

Close assembly

re-open assembly

 

See if that fixes things...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX crashes on inserting section view

Pioneer
Pioneer

Thanks for the replies @Ken_A & @WinnCh !

 

This was ideas converted part and I had to apply Optimize Face command which simplifies surface types (ie. converts b-surfaces into analytic surfaces if possible), merges faces, improves edge accuracy and recognizes blend faces.

It seems to resolve the issue.

 

One catch is Optimize Face will remove any parameters from the feature.