Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX didn't create coordinate datum planes to the new part ?

Genius
Genius

Hello

NX didn't create coordinate datum planes to the new part ?

  • I clicked Create new part inside Assembly and I got this ( Picture ) there are no origo coordinate datum planes ZC, YC, XC where to create a sketch drawing.
  • Do I need to create the "origo datum planes" ?  In Autodesk Inventor the origo datum planes were always there to select. Why NX has no ZC, YC, XC datum planes ?

 

WCS.jpg

 

 

I found this which is the correct TYPE-choise ?

 

dssdsdsd.jpg

1 REPLY 1

Re: NX didn't create coordinate datum planes to the new part ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

@12131444 

When you open your default template part, is there also no CSYS in there.

 

Because the new part is a copy of the default template parts.

When using an Assembly default template there is no CSYS in there.

If you use the model default template there is a CSYS in there.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions