Cancel
Showing results for 
Search instead for 
Did you mean: 

NX drafting

Solution Partner Pioneer Solution Partner Pioneer
Solution Partner Pioneer

How to create dimensions ,such as in the image?

 

Regard..

 

Richard

2 REPLIES 2

Re: NX drafting

Gears Phenom Gears Phenom
Gears Phenom
Use ordinate dimensions. Type "ordinate dimension" in the command finder (without quotation marks) while in the Drafting application to find the command. The Help docs might be useful for details on how to use the command or set up the origin.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.5.1

Re: NX drafting

Siemens Phenom Siemens Phenom
Siemens Phenom

@Richard_audie, As per comment from Tim, you need to use Ordiante Dimension command.

 

I have attached image in which the dimensions are created in same way as per your query. You need to take care of one thing to create such dimensions, Align X and Y axes while creating sketch with default X and Y axes of CSYS then only you will be able to create it.

Regards,
Ganesh Kadole
#IngenuityIsNX | NX - What's New