Cancel
Showing results for 
Search instead for 
Did you mean: 

NX fonts change

Builder
Builder

Hello NX team,

 

can anybody help me, how to change fonts style, size, Bold/ italic style in NX

 

& only software font would change, not for system fonts

 

is there any provision there to change it,

 

appreciate for help

 

 

 

 

Warm Regards
Thomas Roman
Machine Designer
7 REPLIES 7

Re: NX fonts change

Siemens Phenom Siemens Phenom
Siemens Phenom

Re: NX fonts change

Builder
Builder

Hello bro,

 

i do not wanna change my system font ,,

 

i wanna change only NX font & styles,,

 

not for all 

 

thanks

Warm Regards
Thomas Roman
Machine Designer

Re: NX fonts change

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Thomas_Roman,

This is not what you have asked but there is option in user interface preferences.

Menu > Preferences > User Interface (Ctrl+2), where you can change the theme type (which also includes system font).

There is no direct option within NX to change it's font. If there is any way by editing any NX file, someone will surely suggest/mention it.

Re: NX fonts change

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Just to make it clear:

1) Are you asking how to change the font in the menus & NX dialogs?

2) Or are you asking to change the fonts used for drafting/modeling/PMI?

 

Note the menu/dialog font on unix / Apple computers *I believe* can be controlled (or used to be able to be controlled) with an X Windows resource file (or whatever it is called).

This (to my knowledge) was never implemented for MS Windows (other than what others have already suggested)

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX fonts change

Builder
Builder
hello @Ken A

i wanna change fonts of menus n dialog of NX
not to drafting ,sketch etc,

actually i wanna change NX software default fonts size n style not for modules buddy

so if anybody have idea for this help us guys


warm regards
Thomas Roman
Warm Regards
Thomas Roman
Machine Designer

Re: NX fonts change

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
NX will only read changes made to the Windows "system" theme fonts (which can affect many applications).

Select the Windows Start button and select Control Panel. On the "Appearance and Personalization" dialog, select "Personalization: Change the Theme" and then select "Window Color" at the bottom of the dialog.
Select the text you want to change (e.g., Active Window, Normal, Window Text, etc) and then change the Font from the pull down. Choose OK to accept the changes.
In NX, select "Menu > Preferences > User Interface > Theme". Change the NX Theme Type to "Classic with System Font" or "System" to see the changes made to the Windows system above.

Re: NX fonts change

Builder
Builder

Hello@BenBroad

 

thanks for the suggestion, 

 

I wanna only change only NX fonts, but I think now it's very difficult,  not an issue,,, thanks for the help again all guys

Warm Regards
Thomas Roman
Machine Designer