Cancel
Showing results for 
Search instead for 
Did you mean: 

NX handling 2D data imported from dwg

Genius
Genius

Is there a way to speed up NX when working with 2D geometry imported from dwg. I have imported a not very big (about 300Kb) and it takes a lot of time to NX to select, move...

5 REPLIES

Re: NX handling 2D data imported from dwg

Experimenter
Experimenter

Try creating a sketch, projecting the lines and removing the imported data.

Re: NX handling 2D data imported from dwg

Phenom
Phenom

Depends on where the 2D geometry is going. I think there is a setting that allows for the user to turn off the 2D constraint engine to work on large 2D data sets.

Re: NX handling 2D data imported from dwg

Genius
Genius

I projected them in sketch and remove original imported data but still slow when trying to move, copy them. No problem working in other features of my project with the 2D data loaded in screen, as long as I am not editing the sketch. The sketch is a plant layout. Not a big problem but it is strange that this drawing which was quite small and easyly handled in dwg is so slow in NX maybe it is beacuse NX imported a lot of splines insted of other kind of lines.

Re: NX handling 2D data imported from dwg

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

I would do an "info -> Object" on a representative sample of the geometry - see what it is.

Like you say, possibly a change in the DWG inport settings could make life easier...

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX handling 2D data imported from dwg

Valued Contributor
Valued Contributor
Have you tried to turn the import setting to line and arc?