Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX is available for download

Honored Contributor
Honored Contributor
For the new evolution, of continuous release, without version numbers...the non-version numbers, are the most confusing part.
-Dave
NX1867(if it had versions) | Teamcenter 11.6 | Windows 10

Re: NX is available for download

Gears Phenom Gears Phenom
Gears Phenom

@Ken_A wrote:

Oh, maybe we could call it v33 (and 33.1, 33.2, ... then 34.1, 34.2...), and the license file would make sense again !
INCREMENT NX11110 ugslmd 33.0 permanent 19 SUPERSEDE ...           

That would make WAY too much sense and is WAY too simple.  Don't forget with what you're dealing.....Sales AND Marketing.

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.7

Re: NX is available for download

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

And the CAE stuff is called Simcenter 2019.1 and is based on NX 1847.

/Mattias

NX5 -> NX(1847)
I-Deas Master Series 4 -> NX I-Deas 6.4

Re: NX is available for download

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

@Ken_A wrote:
Oh, maybe we could call it v33 (and 33.1, 33.2, ... then 34.1, 34.2...), and the license file would make sense again !
INCREMENT NX11110 ugslmd 33.0 permanent 19 SUPERSEDE ...           

 


The license file is correct, since it is the 33rd major release, remember 7.5 and 8.5 have been major releases too ;-)

We will see if we can get a more traditional numbering scheme, since inventory systems are displaying the MSI version number (18.47.2400.0000 vs 18.51.2602.0000).

How about {four digit year}.{month of feature release}.{month of bug fix release}?

Currently 1847: 2019.01.01, 1851: 2019.01.02 ???

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX12.0.2, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX (1876) | AWC 3.4 Preparing: -

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX is available for download

Experimenter
Experimenter

Hello,

We have NX6. Do you think any upgrade is possible for this version?

Re: NX is available for download

Siemens Phenom Siemens Phenom
Siemens Phenom

@Cozzy , Below link would be helpful to you:

 

 How to upgrade NX 

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: NX is available for download

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

@BenBroad if a company needs to download an older version of NX, beyond the End of Standard Maintenance (EoSM), say like NX10, in order to align with an OEM. Would this be a request to GTAC to gain access to the downloads?

 

Thanks for your detailed posts, they are always informative.

Re: NX is available for download

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@martinm wrote:

If a company needs to download an older version of NX, beyond the End of Standard Maintenance (EoSM), say like NX10, in order to align with an OEM. Would this be a request to GTAC to gain access to the downloads?


Hi @martinm 

 

Correct.  Contact your local GTAC office, explain the exact kits that you need (base, maintenance release, maintenance pack, etc.) and they will take care of the rest.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1876) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX is available for download

Experimenter
Experimenter
If you working with assemblies and mates on NX6, you will find assembly constrains on other releases very frustrating.

Re: NX is available for download

Siemens Phenom Siemens Phenom
Siemens Phenom

The Automatic update doesn't work for me, probably a faulty password.. ( slightly annoying though that NX keeps stating "an update is available, do you want to download" when it has halted "n-times" already.)

So i go the old way, manual download from GTAC.
 But then the installation gives me this: ( See image)
  Isn't 1872 supposed to overwrite the existing install ?
2019-06-26_11-44-08.png

 

Regards,

 Tomas