Cancel
Showing results for 
Search instead for 
Did you mean: 

NX white particles

Experimenter
Experimenter

Hi,

 

I am currently using NX and I seem to be having a graphical error when I move my cursor. As in the image lots of white particles are left behind when I move my mouse around. It looks like some sort of weird snowy effect.

 

I am currently running Windows 7.

Graphics card: NVIDIA NVS 510

NX version: 11.0.2.7

 

My graphics drivers are up to date. Is there anything I can do to fix this it really disrupts my working.

 

 

 

3 REPLIES

Re: NX white particles

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Phesired,

 

Please refer to this thread regarding the NVS device.

 

With some of the non-certified devices it's possible to tweak the 3D settings in the nvidia control panel to prevent this issue (for example, changing the Global Preset from "Base profile" to "3D App - Visual Simulation".  However, since you have a device best suited to efficiently visualize and digest a great deal of information in the financial trading (i.e., 2D) I suspect you might not have an option to change 3D settings.

 

Regards, Ben

Re: NX white particles

Experimenter
Experimenter

How do I navigate to this on the Nvidia control panel I can't seem to  find it.

Re: NX white particles

Siemens Phenom Siemens Phenom
Siemens Phenom

If you don't see it then it's likely that it's not available with your current driver.  To access the control panel I right click my Windows desktop and it's an option on the pop-up menu.  It's also an option in my list of commands in the Windows Control Panel.

 

Regards, Ben