Cancel
Showing results for 
Search instead for 
Did you mean: 

NX

Pioneer
Pioneer

Can we reset NX to it's default position?

4 REPLIES

Re: NX

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

You mean window size/location on the screen?

or XYZ locations in point (or other) dialogs?

or something else?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX

Pioneer
Pioneer
In AutoCAD there is a option Reset Settings to Default which helps to restore everything in initial state when the software installed and in solidworks there is a reset button which helps to restore software in its initial state. so, my question is can we do it in NX 10?

Re: NX

Genius
Genius
Maybe you should have a look at this thread: https://community.plm.automation.siemens.com/t5/NX-Programming-Customization/NXcustom-for-NX10-0/m-p...
We install NX and the installation folder is read-only. All customization were done in scripts similar to the link above.

Re: NX

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Hi,

 

Try this.

If you are using NX 10 go to File->Help->Log File then Find the location of UGII_LOCAL_USER_DEFAULTS.

If you are using NX 8.5 below go to Help on your tool bar and select Log File then Find the location of UGII_LOCAL_USER_DEFAULTS.

 

after this, close NX

open the folder location delete the NX10_user.dpv

( note:NX version will depend on which version of NX will be changed)

Open Nx.

 

The Customer Defaults should be back from the start.

 

Regards,

~Sen