Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Datum for Width Feature of Size

 

How do I attach a datum call out to the arrow of a dimension line so as to make the feature of size a datum feature of size? A datum call out that is exactly in line with the dimension line means that the feature of size is the datum and not simply one side a width feature. So in picture below I'm attempting to select as the terminating object, the intersection of the extension and dimension line. In the subsequent picture, the datum appears aligned with the dimension line which is my intent. However, if I move the dimension line the alignment is lost as shown in the 3rd photo. How do you make the datum dynamically aligned to the dimension line.Capture1.JPGSelecting the area near the interestion of the dimension line and the extension line