Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 How to set all dialogs to state "MORE"

Gears Phenom Gears Phenom
Gears Phenom

Hello Experts,

 

I was forced to upgrade my all-day-working-NX to NX10.

Now I have to configure the virgin NX to behave as the old one (NX8.5.2) in the different points like:

 

- customer defaults,

- visibility of dialog options for all dialogs,

- path settings,

- ....

 

1. Is there a good way to upgrade the setting files and registry entries from NX 8.5.2 to NX10?

 

and in special:

 

2. I guess in NX8.5.2 there was an opportunity to set ALL dialogs to the "MORE" state to get all dialog options in visibility state, may be by using the roll "Advanced with full menus". (I'm not sure, if I could describe it in the right manner.) Here is a picture to see what I mean:

2017-03-20_Dialog Options - MORE_001.png

 

It looks like having set every dialog into "MORE" state means configuring it for every dialog individually. because I couldn't find such a roll.

 

But I can't imagine that's the only way.

 

Who can help?

With best regard, Michael

| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11 | engelke engineering art GmbH, Germany
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution".

6 REPLIES

Re: NX10 How to set all dialogs to state "MORE"

Community Manager Community Manager
Community Manager

Michael, 

 

I'm going to transfer this post to the NX CAD forum, I think there are more people there who will be able to answer this correctly...


Regards,
Ganesh

Simcenter 3D Community Manager
Simulation and Test Solutions

Re: NX10 How to set all dialogs to state "MORE"

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In NX 10, the role you want is named "advanced". It can be found in the palette -> roles tab -> content folder -> advanced.

 

If you search the forum for "customer defaults", you should find some threads about transferring settings when you upgrade.

Re: NX10 How to set all dialogs to state "MORE"

Siemens Phenom Siemens Phenom
Siemens Phenom

Apart from the advanced role you may want to have a look at:

Preferences / User Interface / Options / Default Presentation of Dialog Content, here choose More.

 

Regards, **bleep**

Re: NX10 How to set all dialogs to state "MORE"

Siemens Genius Siemens Genius
Siemens Genius

You might want to also reset your dialog memory to make sure you are getting the More state of the dialogs...2017-03-21 16_59_43-NX 10.0.3.5 - Modeling - [model3.prt (Modified) ].png

 

 

Re: NX10 How to set all dialogs to state "MORE"

Siemens Phenom Siemens Phenom
Siemens Phenom

The best thing to do with your customer defaults part of the question can be found here.

 

Update customer defaults

 

Scott

Betreff: NX10 How to set all dialogs to state "MORE"

Gears Phenom Gears Phenom
Gears Phenom

ScottFelber, JGray, DickBaardse, cowski1, Ganesh_S,

 

thank you for your help.

I will try to follow all of your suggestions.

 

Michael

| Production: NX10; Development: VB, TCL/TK, FORTRAN; Testing: NX11 | engelke engineering art GmbH, Germany
| Kudos for good posts! And if my post answers your question, please mark it as an "Accepted Solution".