Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Plotting issue HP Designjet 130nr

Experimenter
Experimenter

Hello,

I'm experiencing a trouble with plot/print function in NX10. 

I have NX9 and the plot command is perfect, without any init file, I just added a new printer in Printer Administration and the printer do the job

But in NX10, same situation, I hit the print button and nothing happens (both file>print, file>plot)

I can print only in PDF or in another laserjet printer (HP1210).

I tried many ways, but the simple printing function (file>print) should work, but it doesn't do.

I wonder what I have to do to print in HP Designjet 130nr through File>Print command.

I am missing a init file? a SDI base? 

If anyone could help, I appreciate

Regards

1 REPLY 1

Re: NX10 Plotting issue HP Designjet 130nr

Experimenter
Experimenter

Did you ever resolve your problem?

What are the steps you went through?

We recently added a HP DesignJet T520 printer.

So far IT has not set it up for plotting 1:1

I have to export a PDF and plot from that.

 

thanks,

lsl49