Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 - Section curves color is not as it should be

Legend
Legend

Hello all

 

Since we migrated to NX10, my colleage(an old Pro-E guy) is complaining about section curves color when performing a section cut in modeling. He likes to use pure yellow and as you can see in the attached picture, they are not quite looking yellow. It happens when the background is set to graduated with default colors. The constrast is then a very poor and the color is not popping, thus undermining the  usefulness of the option for him.

 

 

2-Section curves color.png

 

Since he is using the same settings as in the previous release (NX8.5), my guess is something must have change in the way the colors for this background are defined in NX10. Does it even make sense?

 

Thanks for your inputs

 

Laurenj.

2 REPLIES 2
Highlighted

Re: NX10 - Section curves color is not as it should be

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

In the command finder, search for "wireframe contrast"; turn this option off (it is a toggle).

Re: NX10 - Section curves color is not as it should be

Legend
Legend

Thanks Cowski!

 

It was exactly what I was looking for! You will never stop to amaze me!

 

Laurenj