03-29-2016 09:06 AM
Hello all
Since we migrated to NX10, my colleage(an old Pro-E guy) is complaining about section curves color when performing a section cut in modeling. He likes to use pure yellow and as you can see in the attached picture, they are not quite looking yellow. It happens when the background is set to graduated with default colors. The constrast is then a very poor and the color is not popping, thus undermining the usefulness of the option for him.
Since he is using the same settings as in the previous release (NX8.5), my guess is something must have change in the way the colors for this background are defined in NX10. Does it even make sense?
Thanks for your inputs
Laurenj.
Solved! Go to Solution.
03-29-2016 09:10 AM
In the command finder, search for "wireframe contrast"; turn this option off (it is a toggle).
03-29-2016 10:11 AM
Thanks Cowski!
It was exactly what I was looking for! You will never stop to amaze me!
Laurenj