Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 Solr Search Index

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi I had to reinstall NX (10 and 11) after Windows crash. Now I can't find the Reuse Library Management option in the Reuse Library Palette, nor the Index Search-On options.

I know it can be a problem related with Solr but I installed the Documentation Server (I think correclty), the Help on line is working as it should and the Solr server seems to be active (see attached snapshot). In the log file I can't find anything about Solr, so I can't understand what the problem can be. Thank you for any hint

 

3 REPLIES 3

Re: NX10 Solr Search Index

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @Laurus,

 

It looks like the doc server and Solr Server are installed correctly. Do not that the default port in the past was 8181, for the docserver as well for solr. But since the new doc server, is has changed by default to 8282 for the documentation, and 8283 for solr (so 2 different ports).

 

Might be you issue have to do with that.

 

Also look at so more info found in our solution center, this might help:

 

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=solr+reuse+librar...

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=solr+reuse+librar...

https://solutions.industrysoftware.automation.siemens.com/view.php?sort=desc&p=1&q=solr+reuse+librar...

 

Kind regards,

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software
Highlighted

Re: NX10 Solr Search Index

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

If the server is not running on the local client but on a shared server, then you need to change the settings for the indexing service to allow access from the clients by changing the Windows service registry.

There is more information in the installation guide.

Stefan Pendl, Systemmanager CAx, HAIDLMAIR GmbH
Production: NX10.0.3, VERICUT 8.2, FBM, MRL 3.1.7 | TcUA 10.1 MP7 Patch 0 (10.1.7.0) | TcVis 11.4
Development: C (ITK), .NET, Tcl/Tk Testing: NX12.0 | AWC 3.4 Preparing: NX12.0

Employees of the customers, together we are strong Smiley Wink
How to Get the Most from Your Signature in the Community
NX Customization - Best Practice Guide

Re: NX10 Solr Search Index

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Thank you