Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 help doesn't work "search" option from Linux server.

Creator
Creator

Hello guys, I have installed NX10 help in a Linux server, that server has java1.7.0. 67 x64.
But when I try to use "search option" doesn't work . I don't get any message error just don't create the search,
Path: http://nx10_documentation/tdoc/nx/10/nx_help/#uid:index

 

Do I need to have java 1.7 installed in my workstation also?

 

Any advice/suggestion will be really apreciated!!

 

Thank you in advance!

 

Rigo

3 REPLIES

Re: NX10 help doesn't work "search" option from Linux server.

Siemens Legend Siemens Legend
Siemens Legend

You are aware that NX10 Help requires a webserver ?
( to free it from the Java version nightmare we had in earlier versions of NX)

 - No i cannot help you with this webserver... - I only know it's mandatory.
  The client will only need to know the web address of the help webserver, no java requirements.

 

Regards,

 Tomas

 

 

Re: NX10 help doesn't work "search" option from Linux server.

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor

If you continue to have problems getting the NX 10 Help and documentation server installed and running properly, please contact GTAC, they are prepared to support this new feature.

NX Design Apps Documentation & Courseware Manager

Re: NX10 help doesn't work "search" option from Linux server.

Valued Contributor
Valued Contributor

I just installed NX 10 help locally on my computer and it works.

 

Here are the steps:

Get the latest 64bit Java    http://www.java.com/en/download/manual.jsp 

 

Get the help install files, which you must have.

Install both the Doc Server and NX Documentation

Reboot.

Delete install files.

 

This works for me with Firefox, Win7, and NX10.

 

Good luck.

Peter