Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 - memory acces violation

Builder
Builder

Hello, after latest update NX10.0.3 (MP02) randomly crash after change application (modeling to drafting, ...).

Now it's a problem for my work!!!

 

NX10.0.3.5 MP02

10 REPLIES

Re: NX10 - memory acces violation

Siemens Phenom Siemens Phenom
Siemens Phenom

Can you please log a call with the hotline and send then a copy of the syslog.

Steve V

Re: NX10 - memory acces violation

Builder
Builder

Ok, I will contact supplier.

Re: NX10 - memory acces violation

Legend
Legend

i haven't been having any issues, but I noticed they took MP02 off of the FTP

 

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.1 / Autoform r7 /WorkNC 2018 r2
Testing:nothing.
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX10 - memory acces violation

Builder
Builder

Unfortunately, we have it installed on all desktops Smiley Sad.

Re: NX10 - memory acces violation

Siemens Phenom Siemens Phenom
Siemens Phenom

I just received an email from SPLM telling me to delete MP02 and to wait for MP03.


Larry Carpenter, P.E.
CAxPLM Architect @ Siemens Molecular Imaging
Past Board Member @ PLM World, Inc,

Re: NX10 - memory acces violation

Phenom
Phenom
Date: 09-mar-2016 13:23:14
IR Number: 7661500
Short Description: Internal errors Memory access violation
 Hi Michael,
I was able to duplicate the errors in NX10 and NX11. I've gone ahead and escalated this ticket to a Problem Report - Priority 1. As soon as I hear back from Development, I'll let you know.

I’m running:

NX 10.0.3.5

NX Phase= 5

NX Patch= None

Michael Fernando


Die Designer
NX 11.0.2.7 + PDW

Re: NX10 - memory acces violation

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Some good advice that I heard years ago was "Don't install the MP releases unless it directly addresses a problem that you are experiencing". It is my understanding that the MP releases are like "hot fixes" for issues that certain customers are having. The MP's get pushed out quickly; once they are thoroughly tested, they get incorporated into the next MR. You are better off waiting for the MR's when possible; otherwise you are essentially a beta tester.

Re: NX10 - memory acces violation

Legend
Legend

I got sick of reloading my role anytime i went into sketcher, thats why I installed it.

 

I'll guess i'll ride it out awhile, no errors sofar... (knocking on formicaas i type)

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.1 / Autoform r7 /WorkNC 2018 r2
Testing:nothing.
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX10 - memory acces violation

10.0.3 MP2 was posted a few days early, and was quickly recalled. Everyone who downloaded it should have received an email with an explanation and instructions to delete their copy.

It should be replaced with 10.0.3 MP3 next week. 

 

If you have already installed MP2, I would avoid loading roles until you get MP3 installed.

Mark Rief
Retired Siemens