Cancel
Showing results for 
Search instead for 
Did you mean: 

NX10 release notes

Genius
Genius

Hello,

 

I am not quite satisfied with the new nx10 help system...

I managed to install the documentation server and the NX10 help.

And I some found out that I have to write "http://HOSTNAME:8181/tdoc/nx/10/nx_help/"

to access the help. But what do I enter to get the release notes?

 

I tried "http://HOSTNAME:8181/tdoc/nx/10/releasenotes/" because under collection there is a folder named like this but it did not work.

 

Any help here?

 

regards,

josch

3 REPLIES

Re: NX10 release notes

Valued Contributor
Valued Contributor

Try the following:

 

http://HOSTNAME:8181/tdoc/nx/10/release_notes/#uid:index

Michael Pinto | Designer
NX11|Windows 10 Enterprise 64bit|HP Z-Book Studio G3 Workstation|Intel XEON E3-1505M|32GB Ram|Nvidia Quadro M1000m w/4GB

Re: NX10 release notes

Genius
Genius
*argh* I missed the underscore...
Thanks, it worked.

Re: NX10 release notes

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @josch,

 

When you have NX already installed you can also find the correct link in the Windows menu --> All programs --> Siemens NX 10.0 --> Release information --> Release notes.

 

When you did not yet installed NX 10.0, I would not install the docs just for the What's new/release notes.

 

You can also check these online: https://support.industrysoftware.automation.siemens.com/general/nx.shtml

 

Hope this helps.

 

Kind regards,

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software