Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 Customized Crosshatch

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi Guys,

 

I´m a bit worried. I want to create a special crosshatch i need. And it must be slectable from the crosshatch defnition files. i got there the file xhatch.chx

 

is there any option how to learn how to create them, any documents?

 

Or is it just that simple and i did not figure it out

 

the files are build like this

 

!
NAME=Electrical Winding
ALTANG,45
SOLID
ALTANG,135
SOLID
!

 

 

I also did not find any infos at the Help which arguments are available

4 REPLIES

Re: NX11 Customized Crosshatch

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Cableguy,

 

Does this help: User-defined crosshatch patterns?

 

Regards, Ben

Highlighted

Re: NX11 Customized Crosshatch

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Speaking of which,

Is there a way to defined curved hatches? (Not just a array of straight dashes).

Thanks,

Jack

Re: NX11 Customized Crosshatch

Siemens Phenom Siemens Phenom
Siemens Phenom

 

It doesn't seem so.  But you can get creative and try to mimic your curves using straight lines to create a complex hatch pattern: Customize Crosshatch Patterns

 

"The concept behind creating a complex hatch pattern is not difficult, but it can be tedious and frustrating. You’ll usually find it best to draw your pattern out in different colors, one per line specification, and then dimension it as I did in figure 3. This makes it much easier to decide which values are required where.  To put things in perspective, AutoCAD’s Escher hatch pattern requires twenty-one line specifications!"

Re: NX11 Customized Crosshatch

Solution Partner Genius Solution Partner Genius
Solution Partner Genius
Thanks, i dont know why i did not find that myself...

Was enough for me