Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 Part Navigator Cancelled “History-Free Mode”

Pioneer
Pioneer

hello.

 

NX11 Cancelled “History-Free Mode”

 

Unable to switch.

 

 

9 REPLIES 9

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @yeqiong,

 

You are correct, history free mode is no longer available since NX 11.0. There is no way to turn this back on.

 

What you still can do, is use "Remove Parameters". Gives you a "dumb" solid again.

 

Kind regards,


Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Siemens Legend Siemens Legend
Siemens Legend

Legacy parts with History Free Mode are maintained but you cannot create any new parts using this method.

 

Regards

 

Paul

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Siemens Phenom Siemens Phenom
Siemens Phenom
Thanks Paul,

That makes the story complete Smiley Happy

Kind regards,
Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Pioneer
Pioneer
Thank you very much, DennisdeBrouwer andbevyboy . Regards YeQiong

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Legend
Legend

Does that mean if you use templates from NX 10 and prior you'll still have history free option?

 

Personally I don't use history free mode, but I have had a few users who did.

Rob Newcomb, CAD/CNC/Simulation manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2019 r1
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Siemens Legend Siemens Legend
Siemens Legend

No it does not. You only will see HF mode if it was set in a part and saved. If you open in NX 11 you will then see it. However if you change it to History Mode you will not be able go back to HF mode unless you do an undo before saving.

 

 

Regards

 

 

Paul

 

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hello,

is anybody know the specific reasson why is it (history free mode) been removed from NX 11.0 ?

 

Regards,

Destian


@bevyboy wrote:

No it does not. You only will see HF mode if it was set in a part and saved. If you open in NX 11 you will then see it. However if you change it to History Mode you will not be able go back to HF mode unless you do an undo before saving.

 

 

Regards

 

 

Paul

 


 

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Gears Phenom Gears Phenom
Gears Phenom

I have always been very critical of this mode, since his debut in NX6 has gradually evolved losing its initial characteristics.
I filled entire threads in Italy, where I work, trying to explain the difference between direct modeling and synchronous modeling.
I also had many doubts about the finality of this mode seeing how it was treated by the same Siemens in two different ways with SE and NX.

Ciao

Cesare

Re: NX11 Part Navigator Cancelled “History-Free Mode”

Siemens Legend Siemens Legend
Siemens Legend

Destian,

I believe the decision was made to remove HF mode because we added most of the functionality such as "Section Edit" in History mode and that a single  fully parameterised, feature based approach was more consistent and a better workflow.

 

Regards

 

Paul