Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 SKETCH GROUPS

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hi,

I have some problems with sketch groups with NX11: as soon as I group a set of curves in a Rigid Sketch group, I get the message "Sketch contains conflicting constraints". But if I look in the Sketch Relations Browser the status is ok for every constraint.

 The same operation (New Sketch Group-Rigid) with the same geometry works without problems in NX10, so I think it may be something related to the new options for sketch groups (Normal, Rigid, Unique, Scalable): I cannot find any documentation about this.

I attach a file .prt with the geometry I want to group and two images, before and after grouping.

Thank you

3 REPLIES

Re: NX11 SKETCH GROUPS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

There are no attachments?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX11 SKETCH GROUPS

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Spoke too soo - attachments in other post with same title.

Mark (or someone) could you delete this duplicate thread?

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX11 SKETCH GROUPS

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

the problem is that if I attach a .prt file I get an error message, because the .prt extension is not a valid one. An automatic message says -correct the attached file and try again-, and so the post is doubled.