Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11-TC11.2.1 Design while creating new revision saves in only one part

Experimenter
Experimenter

Hello,

I have a problem with creating new revision in the NX. While I create new revision of design it saves only in 1 part and I can't choose more parts despite the fact it occurs in more parts. I need to have all parts with old revision updated to new one. Is it possible?

TeamCenter 11.2.2.1 | NX11
2 REPLIES

Re: NX11-TC11.2.1 Design while creating new revision saves in only one part

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Zawrotniak_j,

 

If I understand correctly, you're explaining that you want existing assemblies to load the part you just revised.  Typically your revision rules in Teamcenter define how new revisions are loaded in NX and Teamcenter.  Therefore, assuming you're using a Revision Rule that loads the latest revision, the newly revised part will load when the assembly is sent to NX or when the BVR is sent to Structure Manager.

 

Regards, Ben

Re: NX11-TC11.2.1 Design while creating new revision saves in only one part

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Or are you asking...

I have assemble A, rev 0, which has components C1, C2, C3 which are also at rev 0

 

You want to update A to rev 1

You want C1, C2, and C3 to also update to rev 1

 

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled