Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 - View Popup Menu Customization Issue

Gears Phenom Gears Phenom
Gears Phenom

I've had this issue happening since NX9 & I don't recall which version, but I seem to recall it being reported as fixed between now & then.  What happens is that I customize the View Popup menu in Drafting to be as shown in Fig. 1

Capture1.pngFigure 1Then after working a few hours/days the ordering changes on a whim (see Figure 2) and it's ALWAYS the Expand command that's jumping up to the top.  I just noticed today that Repeat command is also jumping to the top as well. It only does this when commands are added to the View Popup menu.

Capture2.pngFigure 2I've got no clue what's causing this and would like it fixed - it's a real annoyance.

 

 

Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6
2 REPLIES 2

Re: NX11 - View Popup Menu Customization Issue

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @TimF 

 

I've found PR 7261591 which states the issue was fixed in NX 10.0.3 and NX 11.0.  If you're still experiencing the problem in those versions then I'd suggest opening a new IR with GTAC to investigate.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Re: NX11 - View Popup Menu Customization Issue

Gears Phenom Gears Phenom
Gears Phenom
@BenBroad,

Thanks for looking those PRs up. I will try to get this called in at some point - been a bit busy lately.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6