Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX11 connect cage does not select edges

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

 

hi,

I am using the new NX11 commands for Realize Shape, really cool;  a little doubt: in the  'Connect Cage' command, I cannot select edges of an existing body as reference edge for the cage, only curves; filters are ok and the cue line below actually hints "select curve or face edges", but only curves are selected;  is it an enhancement still in progress?