Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 connect cage does not select edges

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

 

connect.pnghi,

I am using the new NX11 commands for Realize Shape, really cool;  a little doubt: in the  'Connect Cage' command, I cannot select edges of an existing body as reference edge for the cage, only curves; filters are ok and the cue line below actually hints "select curve or face edges", but only curves are selected;  is it an enhancement still in progress?

thank you!

2 REPLIES

Re: NX11 connect cage does not select edges

Siemens Phenom Siemens Phenom
Siemens Phenom

You need to have open edges on both the of the bodies to pick face edges.

 

Cannot pick face edge of cylinder.

 

Step1.jpg

 

Deleted top face of cylinder with no heal option and now I can select it.

 

Step2.jpg

 

The final result now

 

Step3.jpg

 

Scott

 

Re: NX11 connect cage does not select edges

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Thank you, I wrongly selected the solid body's edge, with sheet body's it works.