Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 customization of Material Library

Solution Partner Genius Solution Partner Genius
Solution Partner Genius

Hello Folks,

 

I'm desperate... I try to set up a new Material Library for my NX11. I know that I have to set some variables like

 

UGII_PHYS_MATERIAL_LIB_DIR=
UGII_PHYS_MATERIAL_LIB_DATA_DIR=
UGII_PHYS_MATERIAL_LIB_PATH=

 

As well the customer defaults. But I can do what I want, I create a local material for example. after reboot it is gone, delete, now where to find. 

 

Even in the past I could access the library's with the Material Library Manager and select a type Export Material to Library... in NX11 I can't find this type anymore.

 

Even the NX Help did not bring me on, I tried this in nx9 worked, in nx11 not

 

https://support.industrysoftware.automation.siemens.com/docs/nx/nx9/ugdoc/html_files/nx_help/index.h...

 

 

maybe some have a tutorial how to start up in nx11 ...

 

Cheers

1 REPLY

Re: NX11 customization of Material Library

Siemens Phenom Siemens Phenom
Siemens Phenom

The variables you are using are no longer supported 

 

About the material library format used in NX 7.5 and later releases
 

Beginning with NX 7.5, the material library format changed to a MatML XML format. The legacy Physical Material Library environment variables (those variables named with UGII_PHYS_MATERIAL_LIB_*) no longer apply to the material library in NX 7.5 and later releases.

 

Starting with NX 11 or Simcenter 11, the legacy material library .dat format is no longer supported

 

The best place to start is on this page which will give you the information you need to setup material in NX 11.

 

NX 11 Material Help

 

Scott