Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 - extension line angle

Creator
Creator

I have an issue in NX11 how to change the angle of the extension line while defining dimension. In NX9 the setting was available in drafting preferences and also in the dimension settings (see picture)

 

 

In both version NX9 and NX11 the settings are in the same place in the customer defaults, but the single dimension setting in missing. Does anybody know, where to change the extension line angle in NX11 for a specific dimension?

 

 

2 REPLIES

Re: NX11 - extension line angle

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @Dabrowka,

It is right there in the drafting preferences as well as in the dimension settings.extensionangle0.png

 extensionangle.png

 

Regards,
Ganesh
#IngenuityIsNX | NX - What's New

Re: NX11 - extension line angle

Creator
Creator

Hi, I saw it also, thanks. But how to change it for a single dimension without changing the whole properties?

 

Update: Now I checked it. The setting was not available till I changed the value. Then it is also available in the single dimension setting.

 

Thanks a lot!