Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

hello.
NX11 frame selection delay 0.5 seconds.

 

How should I cancel the delay?

 

20 REPLIES 20

Re: NX11 frame selection delay 0.5 seconds.

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Are you referring to pre-highlighting rather than selection?

Try Selection Preferences (Ctrl + Shift + T)
Check your "Rollover Delay". The higher the number the longer the delay.

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration

Highlighted

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

hello,Ben

 

I am referring to the mouse box selection, rectangular selection box will stay on the screen for 0.5 seconds to disappear.

You say "Ctrl+Shift+T" I am very clear, there is no such option.

 

Regards, YeQiong

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello YeQiong,

 

sounds very much like a refresh issue. Which graphics card does your system have?

 

Johannes

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

Hello  Johannes,

 

My graphics card is: GeForce GTX NVIDIA 745

 

I recorded a video, trouble you to see.

 

 

 

 

 

Regards

 

YeQiong

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello YeQiong,

 

Siemens has a graphics certification process in place, which means, that specific graphics cards are tested with NX (and other software) and if all use cases work well, the graphics card along with the tested driver version will be certified.

But: Only Workstation graphics (quadro etc.) are included in the certification process. Geforce graphics are not meant to be used in workstations and therefore not tested/certified. Although most of the use cases tend to work well, some issues might probably occur.

I am afraid that you discovered one... You could try to modify 3D Settings or upgrade the driver, but there is no guarantee for an improvement. It could even result in worse behavior or a broken installation and you won't get any support from GTAC.

Sorry no better answer... Man Sad

 

Find the certification spreadsheet here: Link to Spreadsheet

 

Johannes

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hello @yeqiong,

 

The GeForce GTX card, are Gaming Cards, not meant for 3D CAD applications.

This is probably the cause of this issue.

 

Please check here to see the certified Graphic cards.

http://www.plm.automation.siemens.com/en_us/support/gtac/#lightview%26url=/en_us/Images/Graphics_Cer...

 

You might be able to solve your issue, by using newer (or older) drivers for the graphics card. But no guarantees, and unfortunatly not supported.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hmm, I overlooked @Johannes_H his answer... But the answer is the same!

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX11 frame selection delay 0.5 seconds.

Legend
Legend

Mine behaves the same way as shown in the video, its not . 5seconds, but its definitely different than NX10

I'm using a certified card and driver.

Graphics device:  Quadro K2200/PCIe/SSE2)

 

I'm not using NX11 yet for production so to be honest I didnt notice it. maybe its a setting as has been suggested? I can see how it would get annoying really quick

 

 

 

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX11 frame selection delay 0.5 seconds.

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

It's not related to your graphics device.

 

Selection was enhanced in NX11 to include Circle selection.  Part of this enhancement was to use the display methods already seen with Lasso Selection.  If you've used Lasso selection pre-NX11 you'll notice that the border is thicker and there is a slight delay having completed the lasso.  This display methods are now used for Rectangle and Circle selection and (per development) the behavior you've reported is by design.

 

Regards, Ben

Ben Broad | PLM Enthusiast | Siemens GCSS

NX (v17 - 1872) | Teamcenter (9 - 12)
Value Based Licensing | Adaptive UI | BETA Registration