Cancel
Showing results for 
Search instead for 
Did you mean: 

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

Hello @DennisdeBrouwer  @BenBroad  @Johannes_H

 

I put the computer into the Quadro K2200 graphics card, found that the problem is still. This should not be the issue of graphics cards, you can test it.

 

54.png

 

 

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi YeQiong,

 

sorry I didn't get the fact that you use NX11. NX10 should behave as you expected it.

 

As Ben mentioned, this is working as designed, and there are also upsides to this new behavior.

Objects are now highlighted during Rectangle drag. You can now see what your rectangle selection will include before you finish it.

See Video...

 

Regards,

Johannes

(view in My Videos)

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

hi @Johannes_H 

 

(view in My Videos)

Re: NX11 frame selection delay 0.5 seconds.

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi YeQiong,

 

as Ben and I mentioned before, there are changes in the way NX11 rectangle selection works.

If you feel that this slight delay is a problem, you can contact GTAC. But I am afraid that they may not create a Problem Report for you.

 

Regards,

Johannes

Re: NX11 frame selection delay 0.5 seconds.

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
NX10 does behave the same way - if you use Lasso Selection. NX11 now uses the same display methods for Circle and Rectangle Selection. An Enhancement Request is more suitable, to perhaps include an option to edit the delay.

Ben

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

hi @Johannes_H @BenBroad ,

 

I just wanted to find this option to edit the delay.
So come to you for help.
Thank you very much for the help of the two masters! Thanks again!

 

 

 

Regards

 

 

YeQiong

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

Mine behaves the same way, K4000 Quadro, the problem is that while its detecting what to display it locks up the screen momentarily, then once it highlights, it releases and you can move the rectangle again, if you hesitate slightly it locks up the screen while it calculates what to show for selection. If I try and carry on with my rectangle while locked up, the curser moves off the rectangle, then when it finally selects it jumps right away back to the curser---a little annoying

 

Thanks

Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000

Re: NX11 frame selection delay 0.5 seconds.

Legend
Legend

that's why I don't use the Lasso option, it slows me down too much waiting on it.

I can select faces faster individually or small rectangles.

 

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer

hello @R_Newcomb ,

 

How do you achieve it?

 

 

 

Regards

 

YeQiong

Re: NX11 frame selection delay 0.5 seconds.

Pioneer
Pioneer
It does the same with rectangle selection!
Brian
NX 11.0.2
Win 7 pro 64 bit
quadro k4000