Cancel
Showing results for 
Search instead for 
Did you mean: 

NX11 - keyboard bug ?

Experimenter
Experimenter

Have someone experienced some strange things regarding keyboard function in NX 11.

After upgraded from NX 10 to NX 11 users often experience keyboard buttons are keep pressed. So fx in NX suddenly is just type LLLLLLLLLLLL - if NX11 then is closed it stop doing this

And also ALG GR button seems sometimes be default activated, so it is acting as it is pressed down

 

Any input to this

2 REPLIES 2

Re: NX11 - keyboard bug ?

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Did you tried a other keyboard?


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX11 - keyboard bug ?

Experimenter
Experimenter

Yes - there are more users having problem and even working locally without any external keyboard it happens