Cancel
Showing results for 
Search instead for 
Did you mean: 

NX12 MCD: pneumatic pist

Creator
Creator

Hi,

can someone explain me the meaning of the attributes "Volume Extension" when defining a Pneumatic Cylinder. There are sometimes some errors indicating a "negative extension volume" and the NX-help  does not help this time ...

 

Thx

1 REPLY

Re: NX12 MCD: pneumatic pist

Solution Partner Valued Contributor Solution Partner Valued Contributor
Solution Partner Valued Contributor

Hi,
Volume extension means distance between wall of piston and wall of cylinder in MM. Seems to be that "Volume" is volume but it is distance.

see attached picture: for this example is Stroke=100mm, Volume ext. A=1mm and Volume ext B=99mm

 

Capture.JPG