Cancel
Showing results for 
Search instead for 
Did you mean: 

NX12 topology optimization

Pioneer
Pioneer

Hello,

 

are there some good tutorials for NX12 (NX11.0.2) topology optimization 

or examples for download?

on the web I have only found 3-4 videos...

 

Are there some Webinars for topology optimization now?

 

 

kind regards,

BL

7 REPLIES 7

Re: NX12 topology optimization

Pioneer
Pioneer

...

Re: NX12 topology optimization

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

There are at this moment not a lot of movies for this.
The Topology toolbar is working to go from left to right and fill in everything that is needed for your simulation.

So follow these steps:
1. Select your design space.
2. add material
3. add geometry rules (keep in, keep out, mechanical constrains for simulation)
4. add simulation rules (apply here forces of pressures)
5. Start simulation.

 

 

(view in My Videos)

also if you can to the startup folder that's in the download you will also find a help file of the tool.


Ruud van den Brand
Pre-sales NX CAD
cards PLM Solutions

Re: NX12 topology optimization

Creator
Creator

Hello,

Please, I add Topology optimization from Frustum into my NX 12 (acording the install manual) but when i want start function "Estimate Optimization Parameters" (in "Setup Optimization") the NX shows folowing error: 

 

image.png

 

Can you please advise me what to do?

 

Thank you!

Frantisek S.

 

 

 

Re: NX12 topology optimization

Siemens Valued Contributor Siemens Valued Contributor
Siemens Valued Contributor
@fsedlace
Are you running Windows 7? That might be an issue.
I have the same problem, see: https://community.plm.automation.siemens.com/t5/NX-Design-Forum/NX-Topology-Opt-for-Designers/m-p/44...

Re: NX12 topology optimization

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Hi @fsedlace,

 

Topology Optimization currently only works if the language (UGII_LANG and/or regional settings) is set to English.  Based on your dialog your session is set to Czech, which is not currently supported.  Refer to PR 8971214.

 

Regards, Ben

 

EDIT:

 

Based on @LarsMEriksson comment (and hence IR 9033689), please make sure you have downloaded the latest version of Topology Optimization for NX 12 from the FTP server:
NX 12.0.0 Update 01 - NX30556 Topology Optimization for Designers.zip

Re: NX12 topology optimization

Creator
Creator

Hi BenBroad,

Thank you for quick reply!

I have UGII_LANG set to English but my system (WIN10) is in Czech Smiley Sad.

 

Thank you!

 

Regards, Frantisek

Re: NX12 topology optimization

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor
Did you download and install the latest version?
NX 12.0.0 Update 01 - NX30556 Topology Optimization for Designers.zip