Cancel
Showing results for 
Search instead for 
Did you mean: 

NX1851 - Part list enhancement

Phenom
Phenom

Hi,

can someone explain with some examples of this new enhancement?

part list enh.png

Annotazione 2019-03-09 005316.jpg

 

Thank you..
Using NX1880 and RuleDesigner PDM

Built-in functions for converting units of measure

1 REPLY 1

Re: NX1851 - Part list enhancement

Siemens Phenom Siemens Phenom
Siemens Phenom

Hi @cubalibre00 ,

 

With the “Show Combined Mass for Assemblies” toggle is on, the MASS of an assembly will show as the sum of all the assembly components in the parts list except for components that are not added to Parts List, i.e. due to its suppression, reference or exclusion using attribute.

Also note that when 'Show Combined Mass...' is toggled off, then the sub-assembly will display its individual mass.

Please find below snapshots:

ON.JPG

OFF.JPG

 

Hole, it will be helpful.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!