Cancel
Showing results for 
Search instead for 
Did you mean: 

NX1859 - Drafting preferences command is gone

Phenom
Phenom

Hi,

when I was on NX11 and working on old parts, to use the new drafting customer default setting I have to use the command like the image below.

NX11.png

Now on NX1859 the command goes away.

NX1859.png

How can I set the drafting setting on old parts ?

In modelling, drafting setting pilot sketch dimensions and PMI dimensions and also some weld set.

 

Thank you...

Using NX1867
RuleDesigner PDM

8 REPLIES 8

Re: NX1859 - Drafting preferences command is gone

Siemens Phenom Siemens Phenom
Siemens Phenom
What does it show if you search using command finder?

Re: NX1859 - Drafting preferences command is gone

Siemens Phenom Siemens Phenom
Siemens Phenom
As far as I know, now, NX1847 onwards, Drafting and PMI settings are separated, so you'll find Drafting preferences only in Drafting application.

Regards,
Samadhan

GTAC | NX Help: NX1102 | NX1202 | NX1847
Please mark post as an "Accepted Solution", if it answers your question/is more helpful!

Re: NX1859 - Drafting preferences command is gone

Phenom
Phenom

Guys,

the solution is to go in sketch editing and the drafting preferences are now visible.

Thank you...

Using NX1867
RuleDesigner PDM

Re: NX1859 - Drafting preferences command is gone

Siemens Phenom Siemens Phenom
Siemens Phenom

Samadhan is correct. As of NX 1847 the Drafting and PMI preferences are separated into different  dialogs, and you can only access Drafting preferences from the Drafting application now.

Re: NX1859 - Drafting preferences command is gone

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

NX 1847 - What's New

 

"If you set a PMI preference and there is a corresponding Drafting preference, it is also set. "

 

I edited PMI preferences while using Direct Sketch in Modeling and once I inherited the preferences in the Settings for my sketch dimensions the changes were applied. 

Re: NX1859 - Drafting preferences command is gone

Phenom
Phenom

So the PMI decimal places controls the Sketch Decimal Places now? 

Re: NX1859 - Drafting preferences command is gone

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

@sdeters wrote:

So the PMI decimal places controls the Sketch Decimal Places now? 


So it seems.

 

Drafting preferences don't really belong in Modeling (it's odd that they're still in the STE, but I wouldn't be surprised if that changes soon).  I verified that my changes to the PMI preferences were also set in the Drafting preferences - which confirms what I copied in the tdoc in my previous reply. 

Re: NX1859 - Drafting preferences command is gone

Gears Phenom Gears Phenom
Gears Phenom
@sdeters,

Don't worry, it will change again in 5-10 years when some genius feels that a 3D dimension isn't technically related to a 2D dimension and that's why Sketch settings such as this were a under Drafting Preference in the first place.
Tim
NX 11.0.2.7 MP11 Rev. A
GM TcE v11.2.3.1
GM GPDL v11-A.3.6