Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 - Bounding Box

Solution Partner Phenom Solution Partner Phenom
Solution Partner Phenom

Seen posts here and had customers ask about bounding box functionality in NX.
The answer was to use Journals/NX Open/Grip etc to solve the problem.

NX has a function called Create Box that existed in the Wizards (Mold, Die or Electrode).
Without one of those Wizard licenses, you couldn't use it.

Saw an IR recently (see image below) which says that from NX9.0.3 onwards, you only need a solid modeling license to use the function.

2015-01-06_10-17-20.jpg

Thought it was pretty neat function so we've made a video to show how to access it and how it works: https://vimeo.com/116116872

This video is currently being processed. Please try again in a few minutes.
(view in My Videos)

Also did some testing and NX9.0.2 can also do the same.
NX10 version of Create Box is better as well.

 

*Note from Amy: I embedded your video directly in your post 

Anthony Galante
Senior Support Engineer
PhoenxPLM
10 REPLIES 10

Re: NX9 - Bounding Box

Valued Contributor
Valued Contributor

Nice to know, thanks!

 

Re: NX9 - Bounding Box

Legend
Legend
Thanks for the info on eng-tips. Not sure why I couldnt find the command in command finder. I added the
BUTTON MW_TOOLS_BOX
LABEL Create a Bounding Box
to my personal.tbr and it works nicely.
Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro

Re: NX9 - Bounding Box

Valued Contributor
Valued Contributor

Is there anything with the bounding box that would put the X,Y,Z dimension attributes into the property of the file. Having the box is nice for show but would be better if it would have these included rather than having to go in and manually having to add more things.

Re: NX9 - Bounding Box

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Interesting the expressions that get created.  Perhaps in future some "reference" expressions could get created in addition (with actual block sidie lengths)? (not sure how to do that)

 

In the meantime. perhaps someone could write a "simple, easy to use" journal?

 

Ken

 

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: NX9 - Bounding Box

Siemens Phenom Siemens Phenom
Siemens Phenom

Ken (and everyone) --

 

Check out the eng-tips thread on this topic for a variety of potential solutions for this, including a journal, a couple of KF approaches, and a UDF solution.  :-)

 

http://www.eng-tips.com/viewthread.cfm?qid=377786

 

Taylor Anderson
NX Product Manager, Knowledge Reuse and NX Design
Tel: +1 (602) 441-0683
taylor.anderson@siemens.com

Re: NX9 - Bounding Box

Creator
Creator

Hi PhoeNX,

 

This is not working for me, how do I get past the Mold Wizard license?

 

image.png

Re: NX9 - Bounding Box

Legend
Legend

That function was moved to modeling some time in NX9, are you running the latest release? 

It's been quite a few years since I ran NX9, I'm not sure when they moved that command to Modeling

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro
Highlighted

Re: NX9 - Bounding Box

Creator
Creator

Rob,

 

I am running NX10, did Siemens not continue to have this in Modeling? It's called Bouding Box in NX12 but in NX10 it's Create Box, it still doesn't work for me.

 

-Will

Re: NX9 - Bounding Box

Legend
Legend

I'd contact Gtac if it's not working, at the time, NX9 and NX10 we only had the old ADVDES bundles. Create box/Bounding box was moved into a Modeling license

 

In NX 10 help https://docs.plm.automation.siemens.com/tdoc/nx/10/nx_help/#uid:xid617745

it even lists Modeling

Application

Modeling, Mold Wizard, Progressive Die Wizard

Rob Newcomb, Design and Engineering manager
Elmhirst Industries, Specializing in Prototype sheet metal stampings and assemblies

Production: NX 12.0.2 / Autoform r8 /WorkNC 2020.0
Testing:NX 1855
PC: Rave Cadbeast: Intel(R) i7-4790K CPU @ 4.GHz /32gb ram /NVIDIA Quadro P2000 on Win10 Pro