Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

NX9 Composite feature control frame

Pioneer
Pioneer

Hello,

 

 

a user of mine needs to create a composite feature control frame with three lines.

It seems that in NX9 there are only two available.

Since this is a customer project we have to stick to NX9 (know that it works in NX10).

I`ve tried to create a composite frame with the text editor but cannot work it out.

Does anyone know how to get this frame in NX9?

 

Thanks

 

Klaus

4 REPLIES 4

Re: NX9 Composite feature control frame

Siemens Phenom Siemens Phenom
Siemens Phenom

NX9 only allows 2 frames at a single time.  To get a third frame, create it as a single frame, then drag it below the two row frame until it 'stacks' and 'locks' into position.

Re: NX9 Composite feature control frame

Pioneer
Pioneer

I`m aware of the stacking features in NX but that would not create the same composite frame our users created in other cad systems.

I thought it was possible to create a triple composite frame with the "old" text method.

But in the meantime I confirmed that also there only a double frame is possible.

 

 

Re: NX9 Composite feature control frame

Valued Contributor
Valued Contributor
Hi Klaus,

by older Method in NX is possible it make. But it bringt few disadwantages. Be carefully by using this:
In classic text window put this text in one line and you will see:

<&60><+><&11><+><G0.598>0.05 <G1><+>A<+><&80>0.5<+>C<+>S<+><&80>0.5<+>C<+>S<+><&80>0.5<+>C<+>S<+><&90>


Re: NX9 Composite feature control frame

Pioneer
Pioneer

Hello GrLoki,

 

thank you very much.

it will be hard to modify or recreate by our users but at least it is possible.