Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 Hole callouts

Valued Contributor
Valued Contributor

The holes callouts are very good but I have noticed that in the case of an array of holes it is only the original hole that can be dimensioned.

 

This in now way replects the way in which a designer details up a drawing as available space will dictate which of the arrayed holes is dimensioned.

 

Is there any way of getting wound this?

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12
7 REPLIES 7

Re: NX9 Hole callouts

Siemens Genius Siemens Genius
Siemens Genius

Hi

 

Using NX9.0.1 i don't have a similar behavior.

 

The Drafting / Radial / Hole Callout command lets me select all occurences of a Hole pattern feature.

and not lonly the original.

 

Can you give us more detail ?

Re: NX9 Hole callouts

Valued Contributor
Valued Contributor
Hi

I am creating a hole then using the pattern feature command, then in Drafting using the Radial hole callout.

It will currently only allow me to dimension the original hole but not the instances instances, although it does callout the correct number of holes.

Your say you are using NX9.01, so I will now download that version and give it another go.

Regards
Martyn
--------------------------------------------------------------------------------------------------
This email and any attachments are confidential and are for the use of the
addressee only. If you are not the addressee, you must not use or disclose the
contents to any other person. Please immediately notify the sender and
delete the email. Statements and opinions expressed here may not
represent those of the company. Email correspondence is monitored by
the company. This information may be subject to export control
regulation. You are obliged to comply with such regulations.

Renishaw plc (company number 1106260) and Wotton Travel Limited (company
number 01973158) are companies registered in England and Wales with a registered office
at New Mills, Wotton-under-Edge, Gloucestershire, GL12 8JR,
United Kingdom, Telephone +44 1453 524524.
--------------------------------------------------------------------------------------------------
Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12

Re: NX9 Hole callouts

Siemens Phenom Siemens Phenom
Siemens Phenom

This has been working fine since NX 9.0 was released.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: NX9 Hole callouts

Valued Contributor
Valued Contributor

Eventually got to the bottom of this.

 

The Method has to be set to Variational when doing the array, and not Simple

 

I will go with this, but not sure it make total sense.

Martyn, Principal CAE Engineer, Renishaw PLC
NX12 Tc12

Re: NX9 Hole callouts

Valued Contributor
Valued Contributor

Just saw this thread. It is also this way in NX8.5.3. Apparently they have no intention of fixing this.

Re: NX9 Hole callouts

Siemens Phenom Siemens Phenom
Siemens Phenom

I've brought these issues to the attention of the people responsible for the Drafting funcionality.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: NX9 Hole callouts

Siemens Genius Siemens Genius
Siemens Genius

That's corect, today we support selection of all hole callout instances if the pattern was created as a Variational array and not Simple. We intent to support Simple in the future.

 

Dave