Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9: Sketcher Question

Experimenter
Experimenter

Is there a method to display line number in sketch mode vs. hovering over a line to display as pop up?

 

Creating a sketch and when input section is not valid, one can run a check in which problem lines are identified and their respective problem.  Only issue is, finding the line in a sketch if all lines cannot be turned on for easy viewing and locating...

 

Anyone have any ideas?

2 REPLIES 2

Re: NX9: Sketcher Question

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Preferences -> visualization -> names/borders -> show object names, change the option to something other than "off" (try "all views"). This will display the names of all the named objects on screen at all times. Turn this option off when you no longer need to see them.

Re: NX9: Sketcher Question

Experimenter
Experimenter

Thanks ! Issue resolved!!