Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 flat pattern in NX11

Gears Phenom Gears Phenom
Gears Phenom

Discovered an issue, when I open an NX9 part that contains a flat pattern, and then I go into drafting (same part file) and try to add the flat pattern view, it fails.

 

If I create a sheetmetal part from scratch in NX11, I can add the flat pattern view.  I have also tried deleting the flat pattern, and recreating it in NX11, but it agian fails.

 

I did submit an IR, but curious if anyone else has run into this, or has thoughts on it.

 

Errors below:

ErrorMessage.JPG

-Dave
NX 11 | Teamcenter 11 | Windows 8.1
5 REPLIES

Re: NX9 flat pattern in NX11

Gears Phenom Gears Phenom
Gears Phenom

This is the details of the error message.

details.jpg

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: NX9 flat pattern in NX11

Gears Phenom Gears Phenom
Gears Phenom
Converted to PR 7932450.
-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: NX9 flat pattern in NX11

Experimenter
Experimenter

Was this ever solved?

Re: NX9 flat pattern in NX11

Gears Phenom Gears Phenom
Gears Phenom

Sv1000S wrote:

Was this ever solved?


NX11.0.1 MP3 or higher should do it, 11.0.2 as well.

-Dave
NX 11 | Teamcenter 11 | Windows 8.1

Re: NX9 flat pattern in NX11

Siemens Phenom Siemens Phenom
Siemens Phenom
Was this ever solved?

 

If you're referring to the PR, yes, it was fixed for NX11.0.2 and NX 12.0.

As @DaveK mentioned, also fixed in NX 11.0.1 MP03.

 

Regards, Ben