Cancel
Showing results for 
Search instead for 
Did you mean: 

NX9 "Measure Distance" command disappeared

Experimenter
Experimenter

Surprisingly enough the "Measure Distance" powerfull command doesn't work anymore on my NX-9.03 installation on Win-7-pro.

The "Simple Distance" command keeps poping-up instead of the full"Measure Distance"

Does to anybody happen that?

 

 

4 REPLIES 4

Re: NX9 "Measure Distance" command disappeared

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Start the measure distance command, when 'simple distance' pops up, click on the gear icon in the upper left corner of the dialog box. Choose the option "measure distance (more)", the usual measure distance dialog will appear. Take a measurement and press OK, dialog memory should save the configuration for the next use (the full measure distance dialog should appear the next time you use it).

Re: NX9 "Measure Distance" command disappeared

Siemens Phenom Siemens Phenom
Siemens Phenom

Hallo @facae,

 

Like explained, you can get it back by pressing on the gear in the left top, and select the correct option. This is however a bug, and there is already a PR filed for this issue. It should go back to "Measure distance". This should be fixed in one of the upcoming versions.

 

Kind regards,

 

Dennis

Dennis de Brouwer
Application Support Engineer
GTAC EMEA - Siemens Industry Software

Re: NX9 "Measure Distance" command disappeared

Siemens Phenom Siemens Phenom
Siemens Phenom

I believe it's fixed in NX 10.0.

John R. Baker, P.E. (ret)
EX-Product 'Evangelist'
Irvine, CA

Re: NX9 "Measure Distance" command disappeared

Siemens Esteemed Contributor Siemens Esteemed Contributor
Siemens Esteemed Contributor

Yes John.  I just verified that it behaves correctly in NX10.  It seems like this started happening in NX9.0.3 (PR 2249446).