Cancel
Showing results for 
Search instead for 
Did you mean: 

Naming Clone Assembly

Phenom
Phenom

Ciao to all,

 

I have a Clone Assembly whose files have a suffix '_X' , how can I remove these suffixes?

 

Thanks in advance

 

Cesare

8 REPLIES

Re: Naming Clone Assembly

Genius
Genius

Ciao Cesare,

are you using NX in Native mode or with Teamcenter?

You could try the following: menu->assemblies->cloning and under Naming Tab, select the Define Naming Rule and check if "Add Suffix" is selected. I think it's called Numbering insead of Naming if used with Teamcenter.
Also check the customer defaults, go to Teamcenter Integration for NX --> Part File Name Display and check if a suffix is added.

Re: Naming Clone Assembly

Phenom
Phenom

Thank you @hajnal,

 

I already tried but it does'nt work.

 

Ciao

 

Re: Naming Clone Assembly

Hello,

 

Try Define Naming Rule option.

Define_Naming_Rule.PNG

 

 

 

Thanks and Regards,
Mathi Krishnan.

Re: Naming Clone Assembly

Phenom
Phenom

Thanks @MATHI_CAX_TRG,

 

unfortunately there are more than 200 files all with different name!!!

 

Smiley Frustrated

 

Ciao

Re: Naming Clone Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Try @MATHI_CAX_TRG's suggestion, but in the text to replace option enter the common suffix "_X" (without quotes) and in the replacement text, leave it blank. If it won't allow a blank entry, try entering a space character. A space character at the end of the file name is usually trimmed off before adding the file extension.

Re: Naming Clone Assembly

Phenom
Phenom

Thanks @cowski1,

 

I tried it but a space works only with the Add Suffix option. I also tried to replace with the ALT + 255 character but this character is not trimmed off by the OS....

 

Smiley FrustratedSmiley Frustrated

 

Ciao

Re: Naming Clone Assembly

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

Ok, try this:

Text to replace is "_X". In the replacement text entry, enter a single character such as "~". Specify an output log file and do a dry run (don't do the actual clone). Close the clone dialog. Find and edit the log file (use a plain text editor such as notepad). Near the top of the file, you'll find the naming rule:

&LOG Naming_Rule_Type: REPLACE_STRING Base_String: _X Replacement_String: "~"

Delete the replacement string to create an empty string:

&LOG Naming_Rule_Type: REPLACE_STRING Base_String: _X Replacement_String: ""

Save the log file. Now open the clone dialog and use the "load and apply existing log file".

 

Edit: I tested this on NX 9. Should also work on NX 11?

Re: Naming Clone Assembly

Phenom
Phenom

Great @cowski1,

 

Grazie 10000000

 

Cesare