Cancel
Showing results for 
Search instead for 
Did you mean: 
Highlighted

Nastran *** USER FATAL MESSAGE 300 (RCARD)

Builder
Builder

 

 

Hi All

 

What is this error in Nastran input file when I run it ? in mass matrix for M11 I have a number with negetive exponential like 5-6 , but to whatever number I change , it bugs me with error bellow, how to correct it, or how can I know the total mass ,when I have the mass matrix

 

 

 

*** USER FATAL MESSAGE 300 (RCARD)
DATA ERROR IN FIELD UNDERLINED.
POSSIBLE ERROR IN EXPONENT.
. 1 .. 2 .. 3 .. 4 .. 5 .. 6 .. 7 .. 8 .. 9 .. 10 .
CONM1

1 REPLY

Re: Nastran *** USER FATAL MESSAGE 300 (RCARD)

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

It would probably be better to post this in one of the Simcenter forums

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled