Cancel
Showing results for 
Search instead for 
Did you mean: 

Need help to create complex radius at the blade

Creator
Creator

Hello colleagues,

I need to create radius in the corner on the blade airfoil. But I couldn't find the solution.

Radius should be like the surface after the ball end mill D20R10. Please explain how to create it.

Radius.pngAs it could be

prt. file is here

 

4 REPLIES

Re: Need help to create complex radius at the blade

Siemens Phenom Siemens Phenom
Siemens Phenom

Take a look at the command called blend pocket. 

 

Blend Pocket

 

Scott

Re: Need help to create complex radius at the blade

Siemens Legend Siemens Legend
Siemens Legend

Hi Lassetti,

 

You have a quality issue in your part due to that the two bodies are not lined up properly. This is probably due to the way you have created them. Attached you will find a quick fix as the input geometry only are unparameterized bodies. Have a look to the attached movie file with comments.

 

I hope this will help you

 

Best Regards

Fred

Re: Need help to create complex radius at the blade

Phenom
Phenom

I don't know if this is the solution you are looking for, I trimmed a portion of the bodies to avoid degenerate points and I applied the face blend command as you can see in the attached picture.

Ciao

Re: Need help to create complex radius at the blade

Creator
Creator

Hello Sandman,

Your solution was very helpful! Thank you for the video. It helped me very much!

Also thanks to Cesare, ScottFelber for comments and solution!