Cancel
Showing results for 
Search instead for 
Did you mean: 

New measure command in NX 12.0.1MP01 works only in englisch

Experimenter
Experimenter

Hello

 

The new "Measure" command works only when I switch my NX to englisch.

In german I can't use it, because there is the following infowindow.

Image 2.jpg

 

Is there a way to fix this error.

 

Greatings

Silko

5 REPLIES

Re: New measure command in NX 12.0.1MP01 works only in englisch

Gears Esteemed Contributor Gears Esteemed Contributor
Gears Esteemed Contributor

This should really be reported to GTAC

Ken Akerboom Sr CAx Systems Engr, Moog, Inc.
Production: NX10.0.3.5 MP16/TC11.2
I'd rather be e-steamed than e-diseaseled


Re: New measure command in NX 12.0.1MP01 works only in englisch

Solution Partner Legend Solution Partner Legend
Solution Partner Legend

Doesn't work with the Russian either. Reported to the GTAC with the 'critical' level. Smiley Sad

Re: New measure command in NX 12.0.1MP01 works only in englisch

Experimenter
Experimenter

Hi

 

IR is open with number "IR 9148149" and Siemens can duplicate this.

Siemens will open a PR

 

This is my last Info from GTAC

Re: New measure command in NX 12.0.1MP01 works only in englisch

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

NX 12.0.1 mp01 has been temporarily recalled.  The issue mentioned in this thread was part of the recall.

 

Regards, Ben

Re: New measure command in NX 12.0.1MP01 works only in englisch

Siemens Honored Contributor Siemens Honored Contributor
Siemens Honored Contributor

NX 12.0.1 mp01 has been re-released.  It contains the fix for the issue reported above.

 

Regards, Ben